ABB Adds DC-Input Version to MPR-Series Power Supply Family
- New DC-input version creates additional options for customers looking for compact, high-density, hot-swappable power supplies
- Both compact power supplies provide 700-watt output power
Providing additional input options for customers, ABB is expanding its line of compact, energy-efficient MPR power supplies with a new DC-input version. Both the AC-input and DC-input power supplies feature 9-by-2.15-by-1.57-inch form factors, offering one of the most compact options available today, when it comes to power supply depth.
The MPR0712TE (AC-input version) and MPR0712DC (DC-input version) medium-power units are interchangeable, offering greater flexibility in end application designs that require both input options. The MPR rectifiers achieve power densities of 23 watts (W)/inch and energy efficiencies of up to 94 percent at 50 percent load, achieving an 80 PLUS Platinum grade.
The MPR0712TE features a front 90-to-264-volt AC input, rear +12-volt DC output, and a 700-W output power. The MPR0712DC allows for a front -44 to -72-volt DC input and a rear +12volt DC output with a 700-W output power. Both the AC and DC versions can operate over a wide temperature range of -5 C to 50 C.
The 9-inch long, hot-swappable power suppliles are weel-suited for 12-volt distributed power architecures, mid-end and blade servers, networking equipment and attached storage, routers and switches, as well as advanced workstations. Both the AC and DC versions feature a PMBus*-compliant I2C communications bus, allowing electrical engineers to integrate a range of monitoring and control capabilities into their system designs.
The power supplies are packed with additional features such as active current sharing, remote sensing ability, and a 12-volt standby output voltage. The MPR power supplies also feature built-in overvoltage, overcurrent and overtemperature protections, helping to improve safety and reliability.
To place an order, please click here and search for MPR0712TE (AC-input) or MPR0712DC (DC-input).
ABB (ABBN: SIX Swiss Ex) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s success is driven by about 110,000 talented employees in over 100 countries. www.abb.com
Media Contact:
Matt Falso
ABB Electrification
+1 518 902 5038
matt.falso@us.abb.com