ABB’s new ReliaGear™ LV MCC is the next level in motor control centers
Combining decades of GE Industrial Solutions motor control center (MCC) experience with ABB’s cutting-edge, digital technology in both the ACS580 variable frequency drives and Tmax® XT circuit breakers, ReliaGear™ LV MCC offers the best of both worlds.
ABB today announced the release of ReliaGear™ LV MCC. The low voltage motor control center is built for simplicity and durability. Designed for safety, this low-voltage MCC was created to meet customer needs across a wide range of applications with a focus on smart MCC solutions. ReliaGear LV MCC is UL/cUL 845 listed and available globally in all ANSI markets where NEMA standards are prevalent and/or required.
“Customer feedback started ABB on the journey to build a simple, smart MCC with a wide variety of features and functionality,” said Dick Jackman, Global Product Group Manager for ANSI MV+LV Switchgear, ABB. “The result, ReliaGear LV MCC, brings more advanced protection and controls to the ABB portfolio, enhancing both quality and reliability.”
ReliaGear LV MCC is engineered for use in demanding applications in market segments such as pulp and paper, mining and metals, utility, chemical, oil and gas, mass-production manufacturing, and water and wastewater. The ReliaGear LV MCC motor control center provides a safer, smarter, and more sustainable solution to protect and control motors.
Safer: Retractable stab mechanism allows for closed-door racking, helping keep operators safe from potential arc flash hazards. Integrated surge protection device mitigates risk from surge events, such as lightning, which can cause equipment failure and downtime. Reinforced door latches are 21x stronger than previous designs.
Smarter: ACS580 variable frequency drives are compatible with a wide range of fieldbus protocols meaning the drives, breakers, relays, etc. speak many communication protocol "languages" allowing for easy integration with other systems, including non-ABB systems. Wide range of motor manage-ment relays, including ABB's UMC100.3, allows for communication, protection and control. Tmax XT molded case circuit breakers offer the option for Ekip trip units with added ability for digital protec-tion, management, measurement, and remote monitoring.
Sustainable: Robust design and strong assembly allow for a Seismic Zone 4 standard rating, the most stringent, requiring enclosures to stay intact while experiencing the equivalent of an earthquake measuring up to 8.3 on the Richter scale. Plug starters up to Size 5, allow easy installation and removal. Newly designed disconnect handle is more robust, increasing durability during the life of the MCC.
For more information on features and benefits of ReliaGear LV MCC, please see https://electrification.us.abb.com/products/motor-control-centers.
ABB (NYSE: ABB) is a leading global technology company that energizes the transformation of society and industry to achieve a more productive, sustainable future. By connecting software to its electrification, robotics, automation and motion portfolio, ABB pushes the boundaries of technology to drive performance to new levels. With a history of excellence stretching back more than 130 years, ABB’s suc-cess is driven by about 110,000 talented employees in over 100 countries. www.abb.com
ABB’s Electrification Business Area is a global leader in electrical products and solutions, operating in more than 100 countries, with over 200 manufacturing sites. Our 50,000+ employees are dedicated to delivering safe, smart and sustainable electrification. With ABB AbilityTM enabled digital solutions at its core, our portfolio protects, connects and optimizes the flow of electrical energy for smarter electricity distribution for utilities, industry, buildings, infrastructure and mobility. For more information visit https://go.abb/electrification
—
For more information please contact:
ABB Electrification Media Relations
Melissa London
Phone: +1 919 649 6581
Email: melissa.london@us.abb.com