Contact

Header Top Menu

US Electrification
Powering Connectivity
GE Expands BoostLynx* Voltage Converter Product Family with 130-Watt Additions
Industrial Solutions

Powering Connectivity: GE Expands BoostLynx* Voltage Converter Product Family with 130-Watt Additions

December 5, 2017
Expanded BoostLynx* Offering Increases GE’s Step-up Power Capabilities to Meet the Needs of Today’s Power-Hungry Devices
New 130-Watt Modules Enable Power Conversion from 12 Volts to up to 54 Volts
 
ATLANTA — December 5, 2017 — Building on its existing line of DC-DC boost converters and offering more versatility to board designers, GE’s Industrial Solutions (NYSE: GE) has introduced two new additions to its BoostLynx* product family—ABXS003A3X341-SRZ (a high-voltage version) and ABXS005A4X341-SRZ (its low-voltage counterpart). The additions to GE’s line of non-isolated, high-efficiency DC-DC voltage converters increase the load capacity of the product family to up to 130 watts (W), equipping board designers with a range of solutions to meet the demands of today’s power-hungry applications.
 
The new 130-W BoostLynx modules can convert a standard 12-volt bus voltage (which supports an input voltage range of 8-16 volts) to higher voltages of 16-34 volts with GE’s low-voltage ABXS005 version and to between 32-54 volts with the high-voltage ABXS003 version. The new DC-DC converters join GE’s previously announced 65-W versions to provide more options for board designers faced with ever-evolving power challenges.
 
The easy-to-use BoostLynx converters—also known as point-of-load (PoL) modules—can be used to power any component with an operating voltage between 16-54 volts. For example, the PoL modules could be used in applications such as small-cell remote radio heads, radio frequency power amplifiers, LED backlighting, solenoids and actuators in machinery and automation, fans, surveillance cameras and equipment, sensors and robotics.
 
“The technology we use on a day-to-day basis continues to evolve around us. With these new and improved solutions comes a hunger for more power,” said Vesa Jokitulppo, senior product manager, GE’s Industrial Solutions. “Improving power capabilities and efficiencies of these solutions starts at the board level. By designing embedded components to provide more power and perform better in similar (or, in some cases, smaller) footprints, we are able to help improve the functionality of the end solutions that we have all become so dependent on. It’s what we set out to accomplish with these additions to our BoostLynx product family—which is now able to power any electronic components with an operating voltage of between 16-54 volts.”
 
GE’s fully integrated BoostLynx DC-DC converters use minimal board space, enabling them to provide a high power density of approximately 125 W/inch2. The modules also save space and costs when paired with one of GE’s CLP 150-450-W rectifiers (with an input voltage of between 90-264 volts and an output voltage of 12 volts), as electronic components with both 0.6-5.5-volt and 16-54-volt operating voltages can now be powered from a common 12-volt bus—with a combination of buck and boost PoL converters. In addition, the modules’ flat top inductors make them suitable for conduction cooling—a highly desirable feature in applications with little or no airflow or in demanding thermal environments, and their IPC9592 Class II qualification helps ensure high reliability.
 
“With our new BoostLynx offerings, we are able to provide increased power capabilities without having to overhaul power architectures by stepping up standard 12-volt power to the voltage needed in these power-hungry devices,” Jokitulppo continued.
 
GE’s new ABXS003 and ABXS005 BoostLynx converters now are available, with pricing beginning at $25.03 and $23.39, respectively, at original equipment manufacturer quantities.
 
 
About GE
 
GE (NYSE: GE) is the world’s Digital Industrial Company, transforming industry with software-defined machines and solutions that are connected, responsive and predictive. GE is organized around a global exchange of knowledge, the "GE Store," through which each business shares and accesses the same technology, markets, structure and intellect. Each invention further fuels innovation and application across our industrial sectors. With people, services, technology and scale, GE delivers better outcomes for customers by speaking the language of industry. www.ge.com
 
About GE Power
 
GE Power is a world energy leader that provides technology, solutions and services across the entire energy value chain from the point of generation to consumption. We are transforming the electricity industry by uniting all the resources and scale of the world’s first Digital Industrial company. Our customers operate in more than 150 countries, and together we power more than a third of the world to illuminate cities, build economies and connect the world.
 
For more information, visit the company's website at www.gepower.com. Follow GE Power on Twitter @GE_Power and on LinkedIn at GE Power.
 
* Indicates a trademark of the General Electric Company and may be registered in your region.
 
 
###
 
 
For more information, contact:
 
Sophia Marshall
Global Communications Leader
GE's Industrial Solutions
+1 678 844 5045
 
Matt Falso
Soteryx Corp.
+1 518 886 1076
 

Contact us

Contact us
icon-mail
icon-pin