Contact

Header Top Menu

US Electrification
Two-Hand Control Devices
Industrial Solutions

Two-Hand Control Devices

For machines with manual loading/unloading, our two-hand control devices help keep the operator away from the hazard.

 

 

JSTD-25 Two Hand Control Stations - for use with two Safeball™ 
When two... More

For machines with manual loading/unloading, our two-hand control devices help keep the operator away from the hazard.

 

 

JSTD-25 Two Hand Control Stations - for use with two Safeball™ 
When two Safeballs are used in a two-hand device application, the operator must press all four push buttons simultaneously in order to operate the machine. If one or more of the buttons are released, a stop signal is given to the machine.
For a two-hand control device the operator needs to have a Safeball for each hand to be able to operate a machine. If one or more pushbuttons are released a stop signal is given to the machine.
Two-Hand Control Devices

Related Products

Contact us

Contact us
icon-mail
icon-pin