Contact

Header Top Menu

US Electrification
Specifier Technical Tuesdays
Webinar Sign-up and Archives
ABB
SPECIFIER Technical Tuesdays Webinar
Specifier Technical Tuesdays webinars are held on a Tuesday every month and covers various electrical distribution topics. The archive section below provides access to previous webinars.

 

Webinar Archive

cautionPlease note: The following webinars can be viewed for educational purposes however PDH credits are currently only being issued for participants in the LIVE sessions. ABB is working on offering PDH credits for archived/ on-demand training and will update this website to advise when this service is available.

 

 


 

Medium Voltage Motor Control – Starter Power Components & Starter Types | November 2016

 

 
It is important to understand the components of a medium voltage motor starter, the various types of medium voltage motor starters available, and the difference between medium voltage breakers and medium voltage starters/contactors in order to select and apply the proper medium voltage motor starter for your project. This session will provide you with an understanding of the basic power components of a medium voltage motor starter and their purposes. It will also describe some of the different types of motor starters available.
 
 

 

Low Voltage Motor Control – Starter Power Components & Starter Types | July 2016

 

 
This webinar will describe the components of a motor starter and the various types of low voltage motor controllers in order to select the proper low voltage motor control for your project. This session will provide you with an understanding of the basic power components of a motor starter and their purposes. It will also describe some of the different types of motor starters available.
 

 


 

Power Monitoring – Architectures, Applications & Specification | June 2016

 

 
 
Upgrading or installing a new power system infrastructure is a significant investment. Please join us to discuss how a properly implemented power monitoring system can help maximize this investment. This webinar will discuss:
  • Common power/ energy monitoring architectures
  • Applications that can help quantify, allocate and reduce energy costs
  • How the system can be used as a facilities maintenance tools: Outage analysis, expansion considerations, peak load definition & trending, more…
  • Essential items to include in your specifications 
 

 




Medium Voltage Part 1: Arc Flash Basics - Orgination, Incident Energy Calculations and Impact and Clearing Time on Energy Reduction.  Part 2 Arc Flash Reductions on Low Voltage Substations | May 2016

 

Watch Archived Webinar


Part 1 covered:

  • When/ how arc flash incidents occur and the physical consequences.
  • Bolted vs. arcing faults.
  • Incident energy calculations – quantifying the risk.
  • Effects that clearing time has on energy reduction.
  • Solutions that reduce clearing time such as maintenance switching and zone selective interlocking of instantaneous.

Part 2 covered solutions that can be used to reduce incident energy on the line side of LV main breakers used in equipment such as switchgear or switchboards.

 


 

Metering Fundamentals & Application Considerations | February 2016

 

 
This discussion will educate the participant on the fundamentals and application considerations when providing an electronic meter to meet the customer’s needs. The session will focus on the basic fundamentals of metering, particulars required to properly specify an appropriate electronic meter as well as exploration into various options for each metering scenario and details into the installation in various equipment types.
 

 


 

Medium Voltage Relaying Applications - Differential Protection of Transformers and Switchgear | January 2016

 

Watch Archived Webinar


This discussion will educate the participant in the application considerations & benefits associated with differential protection of medium voltage switchgear and transformers. The discussion will focus on:

• The basics of differential protection – what is it, why use it, different types, benefits and when to use.
• Implementation - how many relays, where are they located, CT style, placement, saturation considerations and quantity.
• Impacts on incident energy reduction.
 

 


 

Design Guidelines for Safer, Low-Voltage Distribution Systems | November/December 2015

 

Watch Archived Webinar


Why is this topic important? The selective coordination of overcurrent devices in low-voltage distribution systems is a very desirable characteristic.  However, designing a system that is both selective and able to react to the currents of arc flash events is very challenging, particularly since it is difficult to predict intuitively what the arcing current will be at a given location without using sophisticated power system analysis software.  The arcing current calculations are just too complex. The guidelines provided in this presentation should help you design your unit substation equipment or low voltage service switchboard in a manner that would achieve the goal of selective coordination and arc flash current sensitivity.

 

 


 

Applying Switchgear vs Switchboards | October 2015

 

Watch Archived Webinar


Why is this topic important? When selecting the proper power distribution equipment for your particular project, it is imperative that the differences between switchgear and switchboard be considered. Good power system design includes knowing when to use switchgear or switchboards based on criteria such as the standards, economics, components, size, application needs and reliability. This session will provide an overview of these differences to help in making those decisions.

 

 


 

Evolution of Medium Voltage Switchgear | September 2015

 

Watch Archived Webinar


Why is this topic important? The increase of medium voltage service drops into facilities is driving user requests for enhanced equipment performance and expanded design capabilities. This webinar will provide an overview of medium voltage switchgear construction and discuss advancements in breaker technologies and design trends that should be evaluated when designing medium voltage switchgear equipment.

 

 


 

 

Applying the NEC 2014 Article 240.87 | August 2015

 

Watch Archived Webinar

 

Why is this topic important? Article 240.87 of the 2014 National Electrical Code requires the use of arc energy reduction methods where low voltage breakers that can be adjusted to 1200A or higher are installed.  This presentation will review how to properly apply this article and discuss important fundamentals related to protection for values of fault current associated with dangerous arcing events.  The focus will be on the implementation and operation of two specific methods cited in Article 240.87 – maintenance switching and zone-selective interlocking (ZSI). The differences between traditional short-time ZSI and instantaneous ZSI will also be highlighted.

 

 


 

 

30-Cyle ATS: Understanding Emergency  System Applications | July 2015

 

Download Presentation

 

Why is this topic important? This webinar will educate the participants in the following areas of the UL 1008 standard for an Automatic Transfer Switch (ATS) Withstand and Close Ratings (WCR). The mandatory and optional test options that exist under the standard; the 3-cycle and optional Short- Time Current Rating (STR) test. How the test options impact the ratings and the robustness of ATS. How a 30-cycle ATS is designed, to supply power to the load after a fault event. Application considerations around why and when to consider the use of a 3-cycle or 30 cycle Short-Time Current rated ATS.

 

 


 

 

Reducing Shock & Arc Hazards in LV Motor Control Centers | June 2015

 

Download Presentation

 

Why is this topic important? In 2014 IEEE incorporated Standard 1683-2014 for Motor Control Centers rated up to 600V AC or 1000V DC. This standard is intended to augment the existing Motor Control Center standards such as, UL 845 or NEMA ICS 18 or CSA C22.2 No. 254 for example, as well as other Motor Control Center design, manufacturing, and application standards. The description states the standard provides recommendations for design practices to reduce the possibility of shock and arcing hazard. Join us to look at some of the design changes and enhancements GE is incorporating in our Low Voltage Motor Control Center product to address the new standard.

 

 


 

 

2016 DOE Transformer Efficiency Changes | May 2015

 

Download Presentation

 

Why is this topic important? The Department of Energy (DOE) regulates the energy efficiency level of low-voltage general purpose dry-type transformers, liquid-immersed and medium-voltage dry-type distribution transformers. Beginning in 2016, there will be newly amended energy efficiency standards for distribution transformers. The new amendments to the existing efficiency standards will further decrease electrical losses thus reducing carbon dioxide emissions. Join us for a technical overview and GE’s interpretation of the new transformer efficiency requirements as they relate to low-voltage general purpose dry-type transformers.

 

 

 


 

Low Voltage Motor Control – Starter Power Components & Starter Types | July 2016

 

 
This webinar will describe the components of a motor starter and the various types of low voltage motor controllers in order to select the proper low voltage motor control for your project. This session will provide you with an understanding of the basic power components of a motor starter and their purposes. It will also describe some of the different types of motor starters available.

Contact us

Contact us
icon-mail
icon-pin