Zenith TruCommand PSG Paralleling Switchgear
Zenith TruCommand PSG paralleling switchgear has become the leader in supplying solutions to simple and very complex systems due to its design flexibility and reliability.
Zenith TruCommand PSG has been providing customer facilities with reliable power switching systems since 1981. Since the inception of paralleling switchgear, many successful Zenith TruCommand PSG installations have been supplied with a focus on providing reliability. Zenith TruCommand PSG has evolved and adapted to the changing technologies in engine generator design, switchgear controls and monitoring systems reflecting ABB's continuing commitment to reliable solutions for critical power applications.
Reliability
Systems in which part of the load is very critical may be best served by paralleling one or more generator sets. Under parallel operation, all the generator sets are started at once. The first set to reach the proper parameters will assume the most critical portion of the load, with the remaining sets picking up lower priority loads. In addition, by using a load shedding application, the failure of one generator set will not interrupt power to the critical loads, as less important loads can be dropped off the line.
Flexibility
Paralleling power sources allow for a wide variety of choices in generation, distribution and utilization of the system's power.
Uninterruptible Maintenance
When one engine - generator set is out of service for maintenance or repair, having others synchronized on the same bus can provide the needed back-up power, should an outage occur.
Cost Savings
Savings can be realized on the application when a number of smaller sets would be less expensive than one large set or when the load makes it impractical to divide into several sections, each with it's own generator. Savings can also occur on the operation side when generator set life is extended from being used only when needed to support the load. Also, when it is anticipated that the load will grow significantly in the future, the capital investment can be reduced by starting with small sets and paralleling additional units as load increases dictate.
Features and benefits
- Intuitive interface makes operation simple. Little or no learning curve required to operate system
- A main screen with navigation buttons and non-system critical button/switches.
- System testing screen allowing the operator to manually initiate automatic system testing operations
- Generator interface settings latched into the PLC control system upon entry
- System load add/shed manual control redundant to hard-wired manual control switches in master control
- Generator optimization settings latched into PLC control system upon entry
- The system is designed to dynamically add or shed load based on the system load level rather than using inflexible load blocks
- The system is programmed to dynamically track the size of each load individually. This allows the system to quickly determine exactly how many loads are to be added to or shed from the system, whether it is in the middle of the afternoon or in the middle of the night
- An ABB governor controller is supplied which has the functionality required by different applications and the flexibility to communicate with all types of existing engines. (Can be used in conjunction with speed controller or can do it itself)
- Build America, Buy America, 2 CFR Part 184, learn more
certifications and Standards
- UL1558 and UL891 designs
- 480 - 15kVA class
- IBC-2005 and IEEE std 693-1997 seismic qualifications
- OSHPD seismic qualifications
- NEMA 1 and NEMA 3R enclosures
Product Scope
- Capable of soft loading and unloading the generator.
- VAR/pf controller built in, load sharing (kW and kVAR).
- Equipped with its own automatic synchronizer that checks for voltage matching.