Skip to main content

Residential Load Center Basics

Load centers are enclosures used to house electrical devices that control and distribute electrical power. A load center is the entry point where electricity from the utility company is distributed throughout a home or building. Load centers are used in residential and light commercial applications where the combined load ranges from 40 to 400 Amps. Many terms are used to describe a residential load center, including breaker box, fuse box, breaker panel, electrical panel, main breaker panel, service entrance panel, circuit breaker box, and circuit breaker panel. It typically includes a main breaker (or switch) that can disconnect all power from the panel, individual circuit breakers or fuses for each branch circuit, and grounding connections. The electric panel's primary purpose is to safely and efficiently distribute electricity while protecting the system from overloads and short circuits.

Load centers, or panels, are like the heart of a home's electrical system. They distribute power from the utility to various circuits throughout the house. This guide breaks down the essentials to help you understand the different types of load centers and their features.

Main Lug vs. Main Breaker Load Centers
  • Main Breaker Load Center:
    Includes a built-in main breaker that serves as the primary disconnect for the entire panel. One switch of this breaker will easily disconnect the entire home from power. The main breaker also protects the panel from overcurrent.

  • Main Lug Load Center:
    Does not have a main breaker. Instead, it’s fed from a breaker upstream (usually from another panel). Main lug load centers are often used as subpanels or in feed-through applications.

  • Feed-Through Main Lug Load Centers:
    These panels allow power to pass through to another load center. They’re useful when: You need to extend electrical service to another building or area, you want to split circuits between multiple panels, or you’re wiring large homes or properties with multiple electrical zones.

NEMA 1 vs. NEMA 3R Load Centers
  • NEMA 1 (Indoor):
    Designed for indoor use in dry locations. These are the most common type of load centers found in basements, garages, or utility rooms. Sometimes, these are found in the hallway, bedroom, or kitchen of a home.

  • NEMA 3R (Outdoor):
    Weather-resistant and suitable for outdoor installations. They protect against rain, sleet, and ice, making them ideal for detached garages or exterior walls.

NEC Service Disconnect Requirement

The National Electrical Code (NEC) requires a service disconnect to shut off all power entering a residence. Below are a couple of key points that should be considered and addressed.

How to Select the Correct Load Center

When selecting a residential load center, it’s important to consider the electrical requirements of the residence. Load center configurations vary based on home size and electrical needs:

Amperage
Circuit Capacity
Typical Use

100A

12–24 circuits

Apartments, small homes

150A

24–30 circuits

Mid-sized homes

200A

30–40+ circuits

Larger homes or homes with electric HVAC, EV chargers, etc.

Specialty Load Centers
What is a Riser Panel?

When constructing a high-rise building, there is a certain kind of load center that makes the most economical and installation sense. This type of load center is known as a riser panel, or floor distribution panel. This load center is installed along an electrical riser, connected to the main service usually on the ground floor. The electrical riser carries power up throughout the high-rise floor by floor. Each riser panel installed on every floor distributes power to the entire floor or portion of the floor through its branch circuits.

What is a Generator Panel?

A main breaker generator panel, or generator subpanel, connects a residential generator with the electrical system of your home. It is the ideal on/off switching system that allows the homeowner to switch between power provided by the electrical utility and the generator. It is typically installed adjacent or close to the main breaker load center. In the event of a power outage, the homeowner can switch power source from the utility to the generator to ensure continuous operation of critical appliances such as lighting, refrigerators, air conditioning and water heaters.

What is Installed Inside of a Load Center?
Surge Protection Devices:

Homes benefit from advanced protection technologies, and the 2020 NEC code now requires the installation of these devices in new construction and replacement/service upgrades.

Whole-Home Surge Protection:
  • Installed inside (THQLSURGE2) or outside of the load center (THOMESUREGE)

  • Protects appliances and electronics from voltage spikes due to lightning or utility surges

Electronic Circuit Breakers:

Any of these circuit breakers comes in both pigtail and plug-on neutral configurations. Learn more about residential circuit breakers.

Thermal Magnetic Circuit Breakers:

Feeder plug-in circuit breakers are also installed in load centers. These circuit breakers provide thermal and magnetic protection from overload and short circuits. When either of these instances is encountered, the breaker will trip as a protection mechanism.

Frequently asked questions (FAQs)

What’s the difference between a main load center and a main lug load center?

Main breaker load centers are typically used as an electrical service entrance. In these setups, the utility’s incoming power cables connect directly to the main breaker, which then distributes electricity throughout the load center and its branch circuits. The main breaker also functions as a primary disconnect and provides overcurrent protection for the entire panel. This powers the whole house.

Main lug load centers are typically installed downstream from a main breaker panel and are commonly referred to as sub panels. Lug load centers connect to the incoming power cables directly to lugs attached to the bus bar, without passing through a main breaker. The "lugs" are terminals that are provided to connect the incoming line. In this case, the main disconnect and overcurrent protection functions must be provided by some other device upstream. Examples include an enclosed circuit breaker, a fusible switch, a circuit breaker in another load center, or a disconnect in a meter enclosure.

Of note, a convertible load center consists of a main lug load center that can be converted to a main breaker in the field.

What is the difference between a load center and a subpanel?

A load center is the main electrical panel used in residential settings. It serves as the main breaker box where electricity from the utility company enters the home and is distributed throughout the entire residence.

A sub panel, or sub panel box, extends the functionality of the main load center by distributing power to a specific area or structure away from the main electrical panel. Often referred to as a small electrical panel, it is used to add circuit capacity, manage electrical loads in separate zones, or provide control for remote areas such as garages, workshops, or outbuildings.

What is the difference between a load center and a substation?

A load center, or main electrical breaker panel, is ideal for standalone installations where no other main disconnect is present and is used for residential or dwelling applications.

A substation plays a critical role in the electrical power system by transforming and switching electricity to ensure a safe and efficient delivery from power plants to consumers. It serves as a connection point between high-voltage transmission lines and lower-voltage distribution networks. Substations are commonly used in industrial and commercial applications where high-voltage handling is required.

What size load center do I need for a typical residential installation?

The size of the load center installed in a home depends on the total electrical load and the household's energy consumption requirements. ABB provides load centers in 40 Amp, 70 Amp, 100 Amp, 150 Amp, 200 Amp, and 225 Amp options. A licensed electrician will assess the specific needs of the dwelling by evaluating appliances, lighting, EV chargers, and other factors. They will calculate the total electrical demand of all connected circuits and devices to ensure it stays within the panel’s amperage rating, while also accounting for future expansion and safety considerations.

Should I install a main breaker or a main lug load center?

Main breaker load centers are typically used as the primary panel in a home, while main lug load centers are used as sub panels for applications like garages, workshops, or outdoor spaces requiring electricity. When used as the primary panel in a home, main breaker load centers provide a means of primary disconnect for the panel. The 2020 NEC code stipulates that a means of outdoor emergency disconnect must be in place, and this can be achieved with an outdoor main breaker load center. Main lug load centers are often smaller and more cost-effective than main breaker load centers. They can also be installed as the primary panel in a smaller home. In order to satisfy code requirements, they are installed downstream from a means of outdoor emergency disconnect. For example, an outdoor main breaker load center, an outdoor meter combo, or an outdoor enclosed circuit breaker will be installed ahead of a main lug load center. Considerations around size, cost, local code, and amperage requirements will come into play when selecting a main breaker or main lug load center.

Are there load centers with integrated surge protection?

Yes, ABB offers residential surge protection to safeguard against power surges and lightning strikes. ABB offers two types of whole-home surge protection. Both offerings are brand agnostic, meaning they can be used with any load center brand. These devices can be installed in load centers and sub panel locations. The THOMESURGE and THQLSURGE2 SPDs provide surge protection for the entire panel and all attached loads. Plus, they comply with NEC®2023.

How many circuits can a load center handle?

The number of circuits a load center can handle varies by model. ABB residential load centers can handle anywhere from 2 to 60 1-inch spaces for the circuit breakers. ABB also sells options for space-saving electrical tandem and quad circuit breakers designed to provide two separate circuits within a one-inch breaker.

What is the difference between plug-on neutral and standard load centers?

Plug-on neutral load centers simplify the installation of arc fault and ground fault circuit breakers (AFCIs and GFCIs) by eliminating the need for pigtail connections. ABB has a ReliaLock plug-on neutral bar to facilitate easy and fast installation.

What are the key considerations for outdoor vs. indoor load centers?

Outdoor load centers need to be weatherproof and rated for outdoor use (NEMA 3R), while indoor load centers (rated NEMA 1) are typically installed in basements, garages, or utility rooms.

 

 

Ask an Expert

Complete the form and we will have an ABB specialist contact you regarding our products and solutions.

Contact us