- General
- Software
Title Sort descending | Date | Size | Publication Number |
---|---|---|---|
In this application note will be explained how to connect and configure a Profinet slave to the 800xA system. A PNQ22.0 with 4 connected UMC motor controller will be used as Profinet slave. |
Date: | Size: 1254871 | Publication Number: 2CDC119019M0201 |
After the installation and the first steps it’s necessary to create a new project in Control Builder M. In this application note is described how to open and save a new project and to configure all connected extension modules to the 800M controller. The second part of this manual is how to update the firmware of the connected extension modules. In the last chapter will be explained how to use the integrated webserver and how to find the connected slaves. |
Date: | Size: 712671 | Publication Number: 2CDC119028M0201 |
Mapping tables for acyclic access to the UMC100.3 - How to access data acyclically |
Date: | Size: 1063646 | Publication Number: 2CDC135068M0201 |
In this Application Note will be described how to set up and create a redundant ring with two Profinet devices PNQ22.0 and four connected UMC100.3 to each device. In addition to that it will be described how to get the diagnostic for each slave. |
Date: | Size: 2742879 | Publication Number: 2CDC135044D0201 |
For some applications only a visualization and the possibility for controlling and monitoring a few devices is needed. In these cases a PLC would be oversized and to expensive. |
Date: | Size: 5968790 | Publication Number: 2CDC135050M0201 |
After updating to Windows 10, it may happen that no UMC100.3 is visible after installing FIM and the UMC device package. This is due to a communication error between the USB terminal and the UMC panel. The root cause is incorrect driver installation. To correct it, the following process must be carried out. |
Date: | Size: 591209 | Publication Number: 2CDC135100M0201 |
Date: | Size: 8209649 | Publication Number: 2CDC135019D0203 | |
The software „Asset Vision Basic” is the frame application for the DTMs of our universal motor controllers. |
Date: | Size: 2483902 | Publication Number: 2CDC135049M0201 |