Skip to main content

    Onsite power today. Grid-ready tomorrow.

    Power at the speed of AI.

    AI is driving data center power demand at unprecedented speed, and new grid capacity takes time to build. Equipment lead times keep slipping, and every month without power is capital sitting idle.

    Onsite power generation closes the gap, but only if every asset works as one. ABB brings together the MV distribution, protection, stability, storage and controls around your generation, so gas turbines, gas engines or fuel cells run as one unified power plant. You have your prime movers on order. We handle everything else.

    With prefabricated, factory-tested E-Houses and skids, and an adaptable execution approach, ABB helps shorten the path from design to first power.

    Outer Wheel Wheel One Unified Control System Synchronous Condenser Excitation System MV Switchgear and Protection HiPerGuard MV UPS ABB Care Lifecycle Partner Prefabricated E-Houses + Skids Plant Optimization Hybrid Energy Storage Digital Offerings Tested in simulation. We simulate your system before it's built.
     
    Select a solution on the wheel to open its product page.
    Operators in a control room monitoring ABB Ability™ System 800xA® screens

    Unified control

    Unified, not just integrated.

    One brain for your entire onsite power plant

    Most onsite plants are pieced together from different vendors' systems joined with adapters and gateways. That's integrated. ABB is unified: electrical and process control run on one backbone, ABB Ability™ System 800xA®, so generation, storage, distribution and protection work as one system with one operator experience.

    Built for power plants. Proven in data centers.

    Everything between your generators and your load

    Generation, storage and grid integration solutions in one unified system

    ABB doesn't sell turbines. We make any turbine work. Click any point on the site to see how our portfolio turns onsite generation into data-center-grade power, from the medium-voltage substation to the control room.

    Rendering of a data center campus with onsite generation and power distribution infrastructure
     
     

    Works with any generation source: gas turbines, gas engines or fuel cells, supplied by you or your OEM.

    Proven starting points. Engineered for your site.

    Every site is different, so these are starting points, not cookie cutters. Both designs are built from modular blocks (generation, stabilization and storage) that you can add or remove as your campus grows. Final ratings and performance are confirmed through system studies for your site.

    Conceptual single-line diagram: gas generation, synchronous condensers and hybrid energy storage on a 13.8 kV ring bus, stepped up to 34.5 kV distribution.

    Reference architecture 1

    Gas turbines + grid stability
    GenerationGas turbines (customer-supplied), 25 MW reference design with N+ redundancy
    StabilityStabilizing assets with flywheel + hybrid energy storage
    Critical power—
    Ideal forFirm, dispatchable capacity, islanded or grid-ready
    Conceptual single-line diagram: fuel cells, synchronous condensers and hybrid energy storage on a 34.5 kV ring bus feeding MV UPS switchgear.

    Reference architecture 2

    Fuel cells + critical power
    GenerationFuel cells (customer-supplied), 25 MW reference design with N+ redundancy
    StabilityStabilizing assets + hybrid energy storage, providing the grid-forming reference fuel cells need
    Critical powerHiPerGuard™ MV UPS for critical loads
    Ideal forLower-emission generation with critical-load protection

    Islanded today? Grid-connected tomorrow?

    Tell us your plan: stay islanded, connect to the grid, or both? And does the transition between modes need to be seamless? ABB designs for every path, including moving from one to the other.

    Talk to an expert to find your architecture

    Built for how you build

    Data hall opening onto an onsite power yard with ABB E-Houses and a transformer being installed

    NeoClouds

    Power at the speed of AI

    Get GPU capacity online on your timeline. Modular building blocks and prefabricated E-Houses compress your path to first power.

    Two engineers reviewing a tablet beside an ABB control panel in a caged colocation hall

    Colocation

    Uptime your tenants can count on

    Meet contracted availability with protection, stability and unified controls designed for mission-critical loads.

    Onsite generation yard with gas engines, fuel tanks and a substation feeding a data center campus

    Developers & IPPs

    One partner, generation to grid

    One accountable partner for everything electrical between your prime movers and your data hall, from engineering studies to long-term service. Simpler contracts, fewer interfaces.

    Contractors installing a prefabricated E-House while a transformer is lifted into place

    EPCs & Contractors

    Fewer interfaces, fewer surprises

    One supplier for MV distribution, protection, controls, storage, stabilization and E-Houses: clear scope boundaries and fewer vendor interfaces.

    Your guide to onsite power generation

    Everything electrical between your prime movers and your data hall, in one guide

    ABB gradient ABB

    Solutions Guide

    Onsite power generation for data centers

    Grid-forming stability for AI data centers

    Insight 1

    Grid-Forming Stability for AI Data Centers

    See how ABB brings onsite generation together in one unified system. The Solutions Guide explains how ABB approaches onsite power, two reference architectures, and the full portfolio behind them.

    What's inside

    • The ABB approach to onsite power
    • Two reference architectures
    • The full portfolio behind them

    Talk to an onsite power expert

    Tell us about your project. An ABB specialist will follow up to discuss your architecture, timeline and simulation options.

    Frequently asked questions (FAQs)

    What is onsite power generation?

    Electricity generated at or near the data center (sometimes called “behind the meter”). It can serve as bridge power until grid capacity is available, as primary power, or alongside utility supply.

    Does ABB supply the generators?

    No, and that’s intentional. ABB works with any generation source and provides everything electrical around it: distribution, protection, stability, storage, controls, E-Houses, engineering studies, commissioning and lifecycle service. Generation, fuel systems, civil works and site installation stay with the owner or EPC.

    Can an islanded system connect to the grid later?

    Yes. ABB architectures can start islanded and add grid synchronization when utility power arrives, including black start and seamless transfer where required. Transition behavior is confirmed through system studies.

    How do you handle AI load swings?

    Stabilizing assets provide physical inertia, hybrid energy storage supplies or absorbs fast power swings, and 800xA coordinates every asset in real time. Response times are project-specific and validated through system studies.