Application and Technical (924)
Title Sort descending | Format | Date | ID |
---|---|---|---|
Dimensions of the mounting fixture for eXplore-C10 has changed, and the common mounting bracket shipped with both screensizes has been updated to be compatible with the changed dimensions. 222.41 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0507 |
113.7 KB |
Format: PDF | Date: | ID: 9AKK107492A9389 |
Download CSV reports on custom destination from
the ABB AbilityTM Energy and Asset Manager via API 6.23 MB |
Format: PDF | Date: | ID: 9AKK107991A2658 |
Increase returns with ABB Cylon® Smart Building Solutions. Optimise revenue and increase sustainability at the same time 14.86 MB |
Format: PDF | Date: | ID: 9AKK108468A3025 |
Early batches of FBTi-7T7-1U1R were shipped with labels showing terminal numbers 23 and 24 twice. This has been corrected to 23,24 and 33,34. 125.47 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0509 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements. 182.66 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0529 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements. 182.17 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0532 |
This release provides security enhancements and improved logging facilities. 151.4 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0543 |
This release provides security enhancements resulting from ABB’s internal continuous improvement approach. 107 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0546 |
Cylon BACnet IP controller firmware has been updated to fix a number of issues. 113.58 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0476 |
Cylon BACnet IP controller firmware has been updated to fix a number of issues. 93.3 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0482 |
Cylon BACnet IP controller firmware has been updated to add Smart Router functionality.
• Support has been added for Full Upload and Download for FBXi, CBXi and FBVi.
• A new product variant, FBXi-X48 has been introduced.
• Modbus limits have been enhanced. • A Unit Free input has been added to the Fusion Air strategy module, which can be used with controller-connected sensors. For this input, the value but not the units are directly displayed on the FusionAir LCD. This could be used, for example, for PM2.5 particulate sensing. 150.24 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0489 |
Zone Temperature Input has been added to the FusionAir module. 107.83 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0493 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements. Also, support has been added for new FBTi-7T7-1U1R controller. 158.86 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0504 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements.
This release adds support for the soon to be released FBTI-6T1-1U1R, FBXi-8R8-X96 and FBXi-8R8-H-X96. 155.04 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0510 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements.
A CBXi-8R8(-H) webpage back-up(.tgz) can now be restored on an FBXi-8R8-X96(-H)
• Enhanced the configurability of the FBXi-8R8-X96(-H) serial ports 98.56 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0520 |
Cylon BACnet controller firmware has been updated to support the FusionAir range of Smart Sensors. 131.19 KB |
Format: PDF | Date: | ID: CYLON_BULLETIN_0474 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements. 147.07 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0521 |
In v 9.3.1 firmware, FBVi/FBTi serial port is “Unassigned” by default. Note: This will be revised in v 9.3.2 or later. 122.51 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0531 |
CVE-2023-0635 and CVE-2023-0636 have been identified as vulnerabilities in ASPECT, specifically the administrative interface. These vulnerabilities are removed as of v 3.07.01. These vulnerabilities are not exposed in a properly configured system. 4.13 KB |
Format: html | Date: | ID: HT0045 |
41.41 KB |
Format: PDF | Date: | ID: 9AKK108466A2975 |
140.39 KB |
Format: PDF | Date: | ID: 1MRS758933 |
The SSL Cert shipped with CXproᴴᴰ versions 1.06.00 and 1.06.01 has expired, disabling Full Upload and Download (FUD) functionality. This bulletin describes how to restore that functionality. 154.06 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0494 |
140.63 KB |
Format: PDF | Date: | ID: 9AKK108470A0443 |
116.79 KB |
Format: PDF | Date: | ID: 9AKK108470A0763 |