Publication Library
Title![]() |
Date | Size | Publication Number |
---|---|---|---|
4 pages. |
Date: 08/09/2010 | Size: 27.27 KB | Publication Number: Double Tie |
7 pages; The intended purpose is to provide the user with the information necessary to make an informed decision on the selection of copper or aluminum conductors within electrical equipment. |
Date: 04/02/2008 | Size: 86.39 KB | Publication Number: Alum-Copper |
This document looks at whether to apply switchgear or switchboards and how to cost effectively use switchboard functionalities. |
Date: 12/17/2004 | Size: 152.67 KB | Publication Number: GEAR-OR-BOARDS |
The choice of using either switchgear or switchboards must be based on many different criteria and the design of the power system requires thought be given to each one. Following are insights into just a few of the differences to help in making those decisions. |
Date: 12/16/2004 | Size: 92.39 KB | Publication Number: APPLICATION |
4 pages. By GE Energy - Industrial Solutions, Canada |
Date: 04/18/2012 | Size: 348.16 KB | Publication Number: ArcFlash-CA |
4 pages. Arc flash is a condition that exists with all pieces of electrical equipment. The real question becomes, how do I reduce the threat? |
Date: 10/01/2009 | Size: 103.9 KB | Publication Number: ArcFlash3 |
The purpose of this article is to point out some of the problems associated with meeting the requirements of providing equipment ground fault protection on multiple-source low voltage distribution equipment, both switchgear and switchboards, and how to contend with them. |
Date: 03/28/2005 | Size: 145.86 KB | Publication Number: MULTI-LOW VOLT |
White Paper - design options discussed can be considered as a discrete layer of improvement to the conventional switchboard design. |
Date: 04/28/2016 | Size: 211.98 KB | Publication Number: DesignConsiderations |
Modern power distribution systems, such as the common double-ended substation, contain multiple power sources integrated within one system. This presents significant complexity to the designer attempting to design a protection system that will not be fooled by circulating neutral currents. This paper describes how the âSingle Processor Concept for Circuit Breaker Protection and Controlâ provides ways to address this sensing problem. |
Date: 12/16/2006 | Size: 558.22 KB | Publication Number: DER-035 |
8 pages. |
Date: 07/23/2012 | Size: 415.93 KB | Publication Number: ESW-IEEE |
In this paper, the authors discuss a unique approach to low-voltage switchgear protection and the process of transitioning this concept to a realworld application. The paper describes the architecture and functionality of this approach and explains how a centrally controlled system can provide advanced monitoring and protection functions much more effectively than existing systems. |
Date: 12/16/2005 | Size: 596.46 KB | Publication Number: DER-038 |
In this paper, the authors explore a protection-and-control architecture based on a single processor that provides all the protection and control functions for a lineup of low-voltage switchgear. How this method of protection changes the paradigm from individual circuit protection to system protection, while cost-effectively and significantly increasing system reliability and protection is discussed. |
Date: 12/16/2005 | Size: 1007.84 KB | Publication Number: DER-037 |
4 pages. Resistance Grounding Systems are used in industrial electrical power distribution |
Date: 09/02/2008 | Size: 56.88 KB | Publication Number: Resistance-Gro |
10 pages. How remote is your switchgear? Shows what GEs Entellisys Switchgear will allow an operator or electrician to do without being in front of the switchgear lineup. |
Date: 11/09/2011 | Size: 938.66 KB | Publication Number: Entellisys-HMI |
3 pages. The goal of this article is to give the reader a basic understanding of what occurs during an arc flash incident, and an understanding of some of the terms used in qualifying the danger associated with such events. |
Date: 11/06/2013 | Size: 203.48 KB | Publication Number: ArcFlash4 |
The authors explore a protection and control architecture based on a single processor that provides all the protection and control functions for a line up of low-voltage switchgear. They demonstrate how this changes the paradigm from individual circuit protection to system protection, while cost-effectively and significantly increasing system reliability and protection. |
Date: 12/01/2005 | Size: 858.58 KB | Publication Number: DER-036 |
7 pages. GE conducted a survey of industry professionals working in facilities related to the oil and gas industry, pulp and paper industry, and power generation. The study results revealed what we called the problematic three As of arc flash. |
Date: 10/01/2009 | Size: 186.31 KB | Publication Number: ArcFlash2 |
GE’s zone selective interlocking with instantaneous protection (I-ZSI) has been developed to provide safety and selectivity at the same time, all the time. Zone selective interlocking schemes are limited to circuit breakers that are a short distance of each other. Selectivity between a circuit breaker and its downstream current limiting device without control signal connections between the two have also been developed. GEs waveform recognition (WFR) algorithm extends the zone of selectivity from the low voltage switchgear down to the low voltage MCCs, panelboards and any other equipment and at the same time reduces the arc flash energy at this equipment to a low level. This feature has no distance limitation. |
Date: 02/07/2013 | Size: 392.66 KB | Publication Number: IZSI-WFR |