Application and Technical (981)
Title Sort descending | Format | Date | ID |
---|---|---|---|
Dimensions of the mounting fixture for eXplore-C10 has changed, and the common mounting bracket shipped with both screensizes has been updated to be compatible with the changed dimensions. 222.41 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0507 |
161.65 KB |
Format: PDF | Date: | ID: 9AKK107492A9389 |
Download CSV reports on custom destination from
the ABB AbilityTM Energy and Asset Manager via API 6.23 MB |
Format: PDF | Date: | ID: 9AKK107991A2658 |
Increase returns with ABB Cylon® Smart Building Solutions. Optimise revenue and increase sustainability at the same time 14.86 MB |
Format: PDF | Date: | ID: 9AKK108468A3025 |
Early batches of FBTi-7T7-1U1R were shipped with labels showing terminal numbers 23 and 24 twice. This has been corrected to 23,24 and 33,34. 125.47 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0509 |
Firmware for FBU-8R8 and FBU-net
This firmware release is an incremental advance on the initial release 1.0.0. It fixes issues found since release and improves the stability and functionality of the FBU system. 114.98 KB |
Format: PDF | Date: | ID: ABB_BLBA_HVAC_BULLETIN_0549 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements. 182.66 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0529 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements. 182.17 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0532 |
This release provides security enhancements and improved logging facilities. 151.4 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0543 |
This release provides security enhancements resulting from ABB’s internal continuous improvement approach. 107 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0546 |
Cylon BACnet IP controller firmware has been updated to fix a number of issues. 113.58 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0476 |
Cylon BACnet IP controller firmware has been updated to fix a number of issues. 93.3 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0482 |
Cylon BACnet IP controller firmware has been updated to add Smart Router functionality.
• Support has been added for Full Upload and Download for FBXi, CBXi and FBVi.
• A new product variant, FBXi-X48 has been introduced.
• Modbus limits have been enhanced. • A Unit Free input has been added to the Fusion Air strategy module, which can be used with controller-connected sensors. For this input, the value but not the units are directly displayed on the FusionAir LCD. This could be used, for example, for PM2.5 particulate sensing. 150.24 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0489 |
Zone Temperature Input has been added to the FusionAir module. 107.83 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0493 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements. Also, support has been added for new FBTi-7T7-1U1R controller. 158.86 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0504 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements.
This release adds support for the soon to be released FBTI-6T1-1U1R, FBXi-8R8-X96 and FBXi-8R8-H-X96. 155.04 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0510 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements.
A CBXi-8R8(-H) webpage back-up(.tgz) can now be restored on an FBXi-8R8-X96(-H)
• Enhanced the configurability of the FBXi-8R8-X96(-H) serial ports 98.56 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0520 |
Cylon BACnet controller firmware has been updated to support the FusionAir range of Smart Sensors. 131.19 KB |
Format: PDF | Date: | ID: CYLON_BULLETIN_0474 |
This is an incremental build from the previous version that fixes reported issues and adds enhancements. 147.07 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0521 |
In v 9.3.1 firmware, FBVi/FBTi serial port is “Unassigned” by default. Note: This will be revised in v 9.3.2 or later. 122.51 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0531 |
CVE-2023-0635 and CVE-2023-0636 have been identified as vulnerabilities in ASPECT, specifically the administrative interface. These vulnerabilities are removed as of v 3.07.01. These vulnerabilities are not exposed in a properly configured system. 4.13 KB |
Format: html | Date: | ID: HT0045 |
41.41 KB |
Format: PDF | Date: | ID: 9AKK108466A2975 |
140.39 KB |
Format: PDF | Date: | ID: 1MRS758933 |
The SSL Cert shipped with CXproᴴᴰ versions 1.06.00 and 1.06.01 has expired, disabling Full Upload and Download (FUD) functionality. This bulletin describes how to restore that functionality. 154.06 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0494 |
1.06 MB |
Format: PDF | Date: | ID: 9AKK108471A1330 |