- Reliable Protection – Adaptive algorithms help reduce incompatibilities while responding quickly to genuine electrical hazards.
- Improved Homeowner Experience – Fewer unwanted trips mean less frustration and greater confidence in home electrical systems.
- Real-World Validation – Models trained on real-world datasets, not simulations, enabling the creation of more accurate and improved algorithms.
- Trusted ABB Quality – Backed by ABB's global leadership in power and electrical protection.
- Easy Installation – Familiar design and installation process requires no special tools or additional training.
- Long-Term Reliability – Built for dependable performance throughout the life of the home.
- Overloads
- Short circuits
- Parallel arc faults
- Series arc faults
- Overloads
- Short circuits
- Ground faults of 5 mA or greater
- Parallel arc faults
- Series arc faults
- The integrated arc-fault protection meets the requirements of the 2026 NEC and beyond while simplifying installation.
Smarter Protection for Modern Homes
As homes become increasingly connected and energy demands continue to grow, electrical protection must evolve to keep pace. ABB is proud to introduce the next generation of residential circuit breakers: ReliaHome® ELITE AFCI and DFCI Circuit Breakers. Powered by adaptive, machine-learning arc-fault technology, these innovative breakers deliver advanced protection while reducing unnecessary interruptions that can frustrate homeowners and generate costly callbacks.
Designed with intelligent algorithms that distinguish normal household electrical activity from genuine hazards, ReliaHome ELITE breakers provide best-in-class safety, reliability, and performance for today's homes—and tomorrow's.
Smarter Protection Through Adaptive Intelligence
Traditional arc-fault protection devices can sometimes struggle to differentiate between harmless electrical signatures and actual hazards, leading to unwanted tripping. ABB ReliaHome ELITE circuit breakers leverage adaptive machine-learning technology to continuously analyze electrical patterns, improving their ability to recognize real threats while maintaining reliable operation.
The result is enhanced safety, fewer disruptions, and a better overall experience for builders, electricians, and homeowners alike.
Why Choose ReliaHome ELITE Circuit Breakers?
ReliaHome ELITE breakers are engineered to deliver intelligent protection that adapts to the evolving electrical demands of modern homes.
Key Advantages
Advanced Protection Options
Arc-Fault Circuit Interrupter (AFCI)
ReliaHome ELITE Combination AFCI breakers are designed to comply with the 2026 National Electrical Code® (NEC®) and beyond. They provide protection against:
Dual-Function Circuit Interrupter (DFCI)
ReliaHome ELITE DFCI breakers combine arc-fault and ground-fault protection into a single device, protecting against:
Technology Designed for Today's Homes
High-Frequency Ground-Fault Protection
Aligned with NEC 2026 and UL requirements, advanced sensing technology uses higher bandwidth detection to identify leakage currents more accurately than older GFCI technologies, helping reduce false trips while maintaining protection.
Machine-Learning Platform
Advanced machine-learning algorithms trained to recognize the difference between true electrical arc hazards and normal household activity.
Familiar Form Factor
ReliaHome ELITE breakers fit within existing installation workflows, using the same footprint and installation process as traditional breakers. No additional tools, retraining, or workflow changes are required.
Reliability by Design
ABB's advanced protection technology is engineered to maintain power continuity whenever possible without compromising safety.
Continuous Improvement
Field insights and diagnostics support future enhancements, helping ABB continue to meet the changing needs of modern homes and electrical systems.
Benefits for Every Stakeholder
For Builders and Contractors: Reduce Costly Callbacks
Project timelines and customer satisfaction depend on reliable installations. ReliaHome ELITE breakers help reduce nuisance tripping through intelligent protection coordination, minimizing service calls and strengthening builder reputations.
For Electricians and Inspectors: Familiar Installation, Advanced Intelligence
Install with confidence using the same footprint and familiar workflow as traditional breakers. No additional training is required, while advanced ABB engineering delivers next-generation protection behind the scenes.
For Homeowners: Safety Without the Frustration
ReliaHome ELITE circuit breakers work quietly in the background, helping protect families from electrical hazards while adapting to modern appliances, electronics, and expanding home energy demands. The result is enhanced safety, fewer interruptions, and greater peace of mind.
The Future of Residential Protection Starts Here
ABB ReliaHome ELITE AFCI and DFCI circuit breakers represent a significant advancement in residential electrical protection. By combining adaptive machine-learning technology with ABB's trusted engineering expertise, these breakers deliver smarter safety, improved reliability, and a better experience for everyone involved—from installation to everyday living.
As homes continue to evolve, ABB is committed to providing innovative solutions that help protect what matters most.