Installation and Instruction (63453)
Title Sort descending | Format | Date | ID |
---|---|---|---|
Detailed specifications for the sample Applications included in CXproᴴᴰ 1.92 MB |
Format: PDF | Date: | ID: MAN0146 |
Guide for configuring and using the CXproᴴᴰ Datalog Manager to visualise Trend Log data from Cylon® BACnet sites 1.49 MB |
Format: PDF | Date: | ID: MAN0136 |
CXproᴴᴰ is backward compatible but not forward compatible. To avoid compatibility issues, the latest release of CXproᴴᴰ must be used whenever possible. 138.83 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0511 |
Instructions for installing and licencing CXproᴴᴰ software 812.83 KB |
Format: PDF | Date: | ID: MAN0147 |
Describes how to set up programs for Keypad and SiteGuide devices connected to Cylon® BMS Sites 855.73 KB |
Format: PDF | Date: | ID: MAN0138 |
Detailed specifications for the Macros included with CXproᴴᴰ 1.69 MB |
Format: PDF | Date: | ID: MAN0143 |
The CXproHD Site Backup Utility (sometimes referred to as Backup) is a module of the Cylon software suite.
The Cylon system consists of hardware controllers linked together to form a ‘Site’, and software on a Supervisory PC. The Cylon software on the PC supervising the Cylon hardware uses data files, which are organised on the PC in a directory structure representing the structure of the Site.
Backup allows this directory structure, and any other relevant files to be archived, so that it can be installed on another PC, or restored to the original PC. 2.04 MB |
Format: PDF | Date: | ID: MAN0137 |
Operation instructions for the Site Organizer module of CXproᴴᴰ. 981.76 KB |
Format: PDF | Date: | ID: MAN0135 |
Operation Manual for CXpro software, used to engineer and commission ABB Cylon® BACnet sites. 9.51 MB |
Format: PDF | Date: | ID: MAN0133 |
Constant parameters can now be downloaded in certain modules without the need to cycle the controller outputs, and the LiveLog dialog has been made more intuitive to use. 296.04 KB |
Format: PDF | Date: | ID: CYLON_BULLETIN_0467 |
Users that have both an expired software license AND a valid HASP license on their PCs when they install the CXproᴴᴰ v1.04.00 release may receive an Expired Licence. This bulletin explains how to fix the issue. 156.45 KB |
Format: PDF | Date: | ID: CYLON_BULLETIN_0470 |
Support has been added for FusionAir Smart Sensor. 315.82 KB |
Format: PDF | Date: | ID: CYLON_BULLETIN_0472 |
Support has been added for FBXi-X48, Full Upload and Download, and changed Modbus limits. 726.21 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0488 |
Additional parameters have been added to the FusionAir module. 185.31 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0491 |
Priority Array data can now be retained across controller reboots. 171.44 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0496 |
Support for the AeroCT mobile app has been added. 258.45 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0502 |
Support added for new FBXi and FBTi variants, and FusionAir module permanent setpoint override feature added. 168.99 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0513 |
Added sample strategies and commissioning capability for the new FBTi-6T1-1U1R controller o CXproHD 125.74 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0516 |
Introducing new CXproHD strategy modules and fixed outstanding issues. 397.23 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0528 |
This CXpro update includes improved handling of smart router connections, adds support for TLS 1.3 and modifies wildcards in BACnet Date Range properties. In addition, several issues have been resolved. 363.12 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0538 |
This update includes new CoV Reader and Multi-State Value modules. 304.98 KB |
Format: PDF | Date: | ID: ABB_CYLON_BULLETIN_0544 |
This update includes a new integrated BACnet explorer that replaces NBpro. 427.55 KB |
Format: PDF | Date: | ID: ABB_SBBA_HVAC_BULLETIN_0550 |
510.83 KB |
Format: PDF | Date: | ID: 9AKK107045A9418 |
11.67 KB |
Format: PDF | Date: | ID: 2CKA000092E2072 |
22.81 KB |
Format: PDF | Date: | ID: 2CKA000092E2139 |